MITSUBISHI ELECTRIC Veranderingen ten goede
Machine Building

Energy Efficiency in Cement Production

26.10.20264 minuten leestijd

Energy costs have become a major factor in the competitiveness of cement manufacturers. As the industry faces increasing pressure to reduce emissions while maintaining productivity, improving cement energy efficiency is no longer just an environmental objective. It is a strategic business priority. From grinding and material handling to kiln operation and process control, every stage of production offers opportunities to reduce waste and improve performance.

Which stages of cement production use the most energy?

Understanding energy use in cement production starts with identifying the most energy-intensive processes. Cement manufacturing requires both thermal and electrical energy, with consumption distributed across several stages.

The highest energy demand is typically found in:

  • raw material grinding,
  • preheating,
  • kiln operation,
  • clinker cooling,
  • final cement grinding.

While the kiln is the largest consumer of thermal energy, grinding processes account for a significant proportion of electricity use. According to the International Energy Agency, clinker production remains the most energy-intensive stage of manufacturing due to the high temperatures required for the calcination process.

How can cement plants reduce energy use in material handling?

Material handling systems often receive less attention than kilns or mills, yet they operate continuously throughout the production process. Conveyors, elevators, feeders, pumps and fans collectively contribute significantly to a plant's electricity bill.

Many facilities still use fixed-speed equipment designed for peak loads rather than actual operating conditions. As a result, systems frequently consume more energy than necessary.

Common optimisation measures include:

  • installing high-efficiency motors
  • optimising conveyor speeds
  • reducing idle running time
  • improving fan control strategies
  • automating material flow management

Automation plays a key role in reducing electricity use by ensuring equipment operates according to real-time production requirements rather than fixed parameters. Similar principles are applied across industrial sectors, including industrial automation in automotive manufacturing. Combined with modern energy saving solutions, manufacturers can improve performance while lowering operating costs.

      Where can variable speed drives support lower energy use?

      Variable speed drives (VSDs) allow motor speed to be adjusted according to process demand rather than running continuously at full capacity. This approach is especially beneficial for equipment whose load varies throughout production.

      By matching motor output to actual requirements, VSDs can reduce energy consumption while improving process control and equipment lifespan. Research published in MDPI Sustainability identifies drive technology as one of the key approaches for improving industrial energy efficiency in cement plants.

      How can energy monitoring help identify losses across a cement plant?

      Many cement plants know that energy savings are possible but lack visibility into where losses occur. This is where energy monitoring in cement plants becomes essential.

      Monitoring systems provide real-time information on energy consumption across production areas, making it easier to identify inefficiencies, detect abnormal equipment behaviour and establish performance benchmarks. There are a few areas that should be monitored, for example motor energy consumption, griding operations or energy use per tonne of cement.

      Modern manufacturers increasingly combine monitoring tools with advanced analytics and automation platforms. Solutions such as Mitsubishi Electric's energy saving solutions help provide greater transparency into plant performance and support data-driven optimisation strategies.

      Which metrics show whether energy-efficiency measures are working?

      Successful energy-efficiency initiatives depend on measurable results. Without clear indicators, it can be difficult to assess progress, identify improvement opportunities, or justify future investments.

      Within energy management in cement manufacturing, companies typically monitor a range of operational, energy and sustainability indicators to evaluate performance. These may include electricity and thermal energy consumption, energy costs, equipment reliability, production efficiency and carbon emissions. Tracking such metrics over time helps operators understand whether implemented measures are delivering the expected benefits and where additional optimisation may be required.

      How can existing cement plants improve energy performance without replacing entire production lines?

      Improving efficiency does not necessarily require a complete plant modernisation project. Many facilities achieve significant savings through targeted upgrades and process optimisation. When planning equipment upgrades or modernising production systems, manufacturers can also explore machine building solutions and the four pillars of machine building for further insights into improving industrial performance.

      Potential improvement measures include:

      • retrofitting variable speed drives
      • replacing older motors with high-efficiency alternatives
      • implementing energy monitoring systems
      • optimising kiln control strategies
      • introducing predictive maintenance
      • upgrading automation systems
      • improving heat recovery processes

      A phased approach often delivers the best results. By establishing a baseline, identifying the largest energy consumers and prioritising high-impact opportunities, cement manufacturers can improve performance while controlling investment costs. Digitalisation also plays an increasingly important role.

      As the industry moves towards lower-carbon production, efficiency improvements will remain one of the most practical and cost-effective ways to support sustainable cement production and accelerate the transition to a green cement factory.

      Sources:

      • IEA, Technology Roadmap: Low-Carbon Transition in the Cement Industry – https://www.iea.org/reports 
      • IEA, Cement: Production, Energy Demand and Emissions – https://www.iea.org/energy-sys
      • Cantini et al., Technological Energy Efficiency Improvements in Cement Industries, Sustainability 13(7), 3810 – https://www.mdpi.com

      FAQ section

      Does cement production use more energy for kiln operation or grinding?

      Kiln operation generally consumes more total energy because of its substantial thermal requirements. However, grinding processes are usually the largest consumers of electrical energy within a cement plant.

      How can energy use be monitored across different areas of a cement plant?

      Energy can be monitored through dedicated energy management platforms that collect data from motors, drives, mills, kilns, fans and auxiliary systems, providing real-time visibility into plant performance.

      What role can variable speed drives play in cement production?

      Variable speed drives allow motors to operate according to process demand, helping reduce electricity consumption, improve control and extend equipment lifespan.

      How can a cement plant assess which energy-efficiency measures to prioritise?

      The first step is to establish a baseline through energy monitoring. Plants can then identify high-consumption assets, evaluate potential savings and prioritise measures that deliver the highest return on investment.

      Can regenerative drives return energy to a cement plant’s electrical system?

      Yes. Regenerative drives can capture energy generated during braking or deceleration and feed it back into the electrical network, helping to reduce overall energy consumption and improve system efficiency.


      Vergelijkbare artikelen


      Onderwerpen

      Machine Building