MITSUBISHI ELECTRIC Veranderingen ten goede
Sustainability

Building more sustainable data centre infrastructure

25.09.20264 minuten leestijd

Data centre energy efficiency is often discussed as a matter of reducing electricity consumption. But it is not the only issue. In reality, it is a question of how the entire facility is designed, controlled and operated.

Energy efficiency as an infrastructure decision

A data center combines several connected systems: IT equipment, electrical distribution, cooling, monitoring, automation and maintenance. Each affects the others. A change in workload can increase heat output, which then contributes to higher cooling demands. Cooling equipment affects overall power consumption, while power availability influences the facility’s capacity to expand. In a way, they are inseparable.

Energy efficiency should therefore be treated as an infrastructure decision rather than a single equipment upgrade. The goal is to deliver reliable performance while maintaining better control over energy use. This approach may require combining dedicated solutions for data center infrastructure with appropriate monitoring and control systems.

Why power management matters

Data center power management determines how electricity is distributed, monitored and used across the facility. Without sufficient visibility, operators may know how much energy is consumed but not which systems are responsible for changes in demand.

Monitoring can help identify:

  • where energy is being consumed;
  • how demand changes over time;
  • which systems create the greatest load;
  • whether equipment operates within expected parameters;
  • where maintenance or optimisation could reduce waste.

This information supports more accurate capacity planning and helps organisations prioritise investment. It can also support the implementation of smart energy management for industry across connected infrastructure.

Sustainable data centers

Sustainable data centers must support digital growth without treating energy demand as unlimited. This requires balancing availability, performance, cost and environmental impact.

Sustainability should be considered at three levels:

facility level — energy supply, electrical efficiency and cooling design;
system level — monitoring, automation and integration;
operational level — maintenance, performance reviews and capacity planning.

A sustainable data centre strategy should therefore answer practical questions such as which systems use the most energy, which losses can be measured and reduced, can the available power capacity support future requirements, which improvements can be made without compromising resilience etc.

These questions turn sustainability from a broad ambition into an operational programme.

Improving power management and cooling efficiency

Data centre power management becomes more effective when operators can see the relationship between supply, demand and performance. Measurements should be collected at the appropriate level of detail, allowing teams to identify both overall trends and specific sources of inefficiency.

Inefficiency may result from many different factors such as poor airflow, unsuitable control settings, ageing equipment, inadequate monitoring or a mismatch between cooling capacity and actual demand.

Data center cooling efficiency can be improved through:

  • effective airflow design;
  • suitable cooling equipment;
  • temperature and humidity monitoring;
  • responsive control systems;
  • regular maintenance;
  • analysis of cooling demand alongside IT workload.

The aim is not to reduce cooling at the expense of reliability. It is to provide the required thermal conditions without operating equipment harder or longer than necessary.

Automation, AI and renewable energy

Automation can help operators manage relationships between energy, equipment and environmental conditions. Sensors and control systems provide information, while software can support decisions, issue alerts and adjust selected parameters.

AI and advanced analytics may support demand forecasting, anomaly detection and predictive maintenance. However, technology alone does not create energy efficiency. Its value depends on data quality, reliable control architecture and a clear operational objective.

Renewable energy can support sustainable data center infrastructure, but it does not remove the need to reduce demand. Efficiency, monitoring, maintenance and capacity planning remain essential to long-term sustainable data center operations.

Renewable energy and carbon reduction

Renewable energy for data centres can support efforts to reduce carbon emissions, particularly when integrated into a wider energy strategy. The most appropriate solution depends on local conditions, energy availability, storage requirements and the operating profile of the facility. These considerations are part of broader solutions for energy systems.

Renewable sources should not be viewed as a substitute for energy efficiency. A facility that uses energy inefficiently will still require more generation capacity, storage or purchased electricity. Reducing demand first can improve the effectiveness of renewable energy investments.

Sustainable infrastructure may therefore combine:

  • lower energy demand;
  • efficient electrical systems;
  • optimised cooling;
  • renewable energy procurement or generation;
  • energy storage where appropriate;
  • monitoring and control across the facility.

Measuring progress

Data centre sustainability strategies need clear measures. Operators should track energy use alongside workload, availability and operating conditions. A reduction in total consumption may not represent an improvement if computing output has also fallen. Equally, higher energy use may be justified if it reflects a significant increase in useful computing capacity.

Measurement should support decisions rather than become an administrative exercise. Regular reviews can reveal whether improvements are delivering the expected result, whether equipment performance is changing and where further optimisation may be possible.

The future of sustainable data centre operations

The future of sustainable data centre infrastructure will depend on the ability to connect systems that have traditionally been managed separately. Power, cooling, automation and maintenance data can provide a more complete picture of facility performance.

This connected approach can help operators improve energy efficiency without losing sight of reliability. It can also support more informed decisions about expansion, equipment replacement and long-term infrastructure planning.

The most effective path will vary from one facility to another. The starting point is consistent: measure actual performance, identify the systems that influence energy use and use automation where it can create a clear operational benefit.

More efficient data centres will not be defined by one technology. They will be built through better coordination between infrastructure, data and people.

FAQ section

What is data centre power management?

Data centre power management is the monitoring, distribution and control of electrical energy used by IT, cooling and supporting infrastructure.

How can data centres reduce energy consumption?

They can improve electrical efficiency, optimise cooling, monitor performance, automate control processes and identify equipment or systems that consume more energy than required.

What are energy-efficient data centres?

Energy-efficient data centres deliver the required computing and cooling performance while limiting unnecessary energy use across the facility.

Why is cooling important for data centre sustainability?

Cooling systems can have a major effect on total facility energy consumption. Better airflow, control and monitoring can help deliver the required thermal conditions more efficiently.

Can renewable energy make a data centre sustainable?

Renewable energy can support sustainability objectives, but it should be combined with efficient infrastructure, monitoring and demand reduction.

What is intelligent power management?

Intelligent power management uses measurement, software, automation and control systems to understand and respond to changing energy requirements.

How can automation improve data centre energy efficiency?

Automation can connect operational data with control actions, helping operators detect changes, adjust systems and support predictive maintenance.

What role can AI play in data centre energy optimisation?

AI can analyse operational data to identify patterns, forecast demand and detect abnormal conditions. Its effectiveness depends on data quality and appropriate integration.

How should data centre energy efficiency be measured?

It should be measured using facility and IT energy consumption, cooling demand, peak loads and performance relative to computing output and operating conditions.


Vergelijkbare artikelen


Onderwerpen

Sustainability